Hi,
We are planning to buy 1046ARDB and try to develop application on REDHAT 7.x operating system. I am having doubt on the installation of Qoriq Sdk2.0 for LS1046ARDB board. Is the procedure will be same as like installing sdk in the Ubuntu 16.04. Is it will support ?. If it will support, what procedure I need to follow for that Redhat OS.
Kindly please guide me.
Thanks and Regards,
Jayasurya.
Agenslot77 Merupakan situs slot online terbaik sepanjang masa di Indonesia karena Agenslot77 merupakan situs judi terlengkap dan terpercaya yang sudah memiliki ribuan member aktif telah bergabung di situs ini.Agenslot77 juga merupakan situs penyedia layanan slot online,live casino,judi poker,judi bola dan judi togel tergacor sepanjang masa.
Yocto Project supports typical Linux distributions: Ubuntu, Fedora, CentOS, Debian, OpenSUSE, etc. More Linux distributions are continually being verified.
This SDK has been verified on following Linux distributions: Ubuntu 14.04, CentOS-7.1.1503,
Debian 8.2, Fedora 22 and OpenSUSE 13.2
Please download QORIQ-SDK-2.0-IC-REV0 from https://www.nxp.com/, then refer to the following sections.
3.2.1 Install SDK V2.0-1703
3.2.2 Install SDK 2.0
3.2.3 Set Up Host Environment