How to build Optee Application on Hikey960

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build Optee Application on Hikey960

986 Views
nxf36763
NXP Employee
NXP Employee

How to build Optee Application on Hikey 960 platform.

can someone suggest with proper steps.

As we are able to generate the .ta file and executable but, after running TEE-Supplicant it is not able to load executables.

0 Kudos
Reply
1 Reply

831 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ashish Manohar,

Please refer to the example in OP-TEE Trusted Application on QorIQ ARM Based Processors .

CA source code is in optee_storage/host folder, teec_uuid is defined as the following this value is used to open the specific TEEC session.
TEEC_UUID teec_uuid = {
0x59e4d3d3, 0x0199, 0x4f74,
{ 0xb9, 0x4d, 0x53, 0xd3, 0xda, 0xa5, 0x7d, 0x73 }
};

TA source code is located in optee_storage/ta, please refer to the following TEE_UUID definition.
#define TEE_UUID { 0x59e4d3d3, 0x0199, 0x4f74, \
{ 0xb9, 0x4d, 0x53, 0xd3, 0xda, 0xa5, 0x7d, 0x73 } }


Please refer to the following definition in TA Makefile.
BINARY = 59e4d3d3-0199-4f74-b94d-53d3daa57d73

$ make TA_DEV_KIT_DIR=<optee_os path>/out/arm-plat-ls/export-ta_arm64 TEEC_EXPORT=<optee_client path>/out/export
Final CA image and TA image,
CA: host/storage-test
TA: ta/59e4d3d3-0199-4f74-b94d-53d3daa57d73.ta
Copy TA image to /lib/optee_armtz/ and CA to root file system.
$ tee-supplicant /dev/teepriv0 &
$ ./storage-test > log

Thanks,

Yiping

0 Kudos
Reply