How can I boot a device with p1022 processor from emmc device ? is it possible?
While reading the QorIQ SDK 1.8 manual, I understood that we can place the ext2 filesystem and kernel on the SD card, then the kernel can boot up automatically after the board is powered on, given that parameters in u-boot are set. So. I understood that we can place kernel and file system in sd card.
Where is u-boot stored ?
Can we place u-boot in sd card ?
How to program u-boot. ?