I am currently trying to follow the Freescale guide for booting from an SD card here http://cache.freescale.com/files/32bit/doc/app_note/AN3659.pdf
However, I am mostly struggling to locate all of the prerequisite files at this time:
If I were to be in possession of all these files, I am fairly confident I can run through the instructions with ease, it is just a case of finding these files in the first place which appears to be the trouble.
Could anybody tell me where I can get each of the above please?
Thank you,
Mike
Hello Mike Green,
All these image could be built from QorIQ SDK. Also there are pre-built images in the SDK.
Linux® SDK for QorIQ Processors v1.8|Freescale
Regards
Lunmin
Do you mean that these files are required simply to build an image for flashing to the SD Card? If so, does this mean I could simply use one of the pre-built images on the SDK to boot the P2020 from?
I have looked at the SDK before and came across those pre-built images. How exactly do I go about using those pre-built images on the P2020 once I have found them?
Hello Mike Green,
Sorry for late reply.
Yes, if you use official Demo board, you could directly use those pre-built images.
Have a great day,
Lunmin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------