Does T4240 support ppc64le architecture like IBM's POWER8? I want to run Nvidia's CUDA on T4240

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does T4240 support ppc64le architecture like IBM's POWER8? I want to run Nvidia's CUDA on T4240

跳至解决方案
1,022 次查看
18911073233
Contributor I

I want to run Nvidia's CUDA library on T4240 , Nvidia says CUDA library is ready for x86_64 or ppc64le.

0 项奖励
回复
1 解答
866 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

The e6500 cores of the T4240  have ppc64 architecture. Although it supports little endian functionality, it does not fully implement the necessary instructions in way like Power8 processor which has ppc64le architecture.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
867 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

The e6500 cores of the T4240  have ppc64 architecture. Although it supports little endian functionality, it does not fully implement the necessary instructions in way like Power8 processor which has ppc64le architecture.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

866 次查看
18911073233
Contributor I

Thank you, got it!

0 项奖励
回复