Question
How do I generate an SD card image in Yocto for the LS1043ARDB? I've read about the WIC tool and I see some wks files for the IMX processors, however, I don't see any for the layerscape parts. My issue is that the QorIQ memory layout doesn't seem compatible with WIC ( I could be mistaken). Options like --offset and --align are in (Kbyte boundaries), but the RCW+PBL+BL2 starts at 0x8. Is the WIC tool the right way to go?
Current Status
I have an image that works with a Yocto generated bootloader, dt, kernel, and file system. I want Yocto to create an sdcard image that will place them in the proper places in memory.
Solved! Go to Solution.
Problem solved, on reading the guide closer the memory layout for the SD card is described in block numbers and not a physical address.
Problem solved, on reading the guide closer the memory layout for the SD card is described in block numbers and not a physical address.