Can we use mt25qu512a (quad spi ) in lx2160a?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use mt25qu512a (quad spi ) in lx2160a?

852 Views
DohwanAhn
Contributor II

We made a new board.
The new board is equipped with mt25qu512a, 4bit (quad spi).
However, as far as I know xspi is supported on the lx2160ardb board. (xspi - 8bit bus)
Also, the datasheet of lsdk_20.04 says that lx2160a only supports xspi (qspi is not supported). Also, only xspi is supported in flex-builder. So, we can't build with qspi. Can you give a clear answer on this one? Can we use mt25qu512a for lx2160a?

Can lx2160a load data from flash of 4bit bus (quad spi - mt25qu512a) during initial booting?

0 Kudos
Reply
2 Replies

821 Views
DohwanAhn
Contributor II

Through the reference manual, I saw that xspi works dynamically.

Thanks to your comments.

0 Kudos
Reply

836 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @[Do Hwan Ahn]​,


The LX2160 Flex SPI supports Quad mode. In Quad mode, flash transmit/receive data on 4 Data pins (SIO0~SIO3 for both transmitting and receiving). You can use MT25qu512a.


Refer to chapter#18 in LX2160A reference manual for detailed description.


Regards,

Mrudang Shelat

0 Kudos
Reply