issue about patches for ISI errata ERR050145

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

issue about patches for ISI errata ERR050145

1,560件の閲覧回数
xu_ji1
Contributor V

Hello,

 

After I merged this patch about kernel L5.10,I test single camera capture case is ok,but multi camera capture case,and memory overwrite issue also happened,and log shows error happened about this patch:

[ 1098.672578] bypass csc
[ 1098.674948] input fmt YUV4
[ 1098.678050] output fmt YUYV
[ 1098.680947] mxc-isi 58130000.isi: input_size(1280,720), output_size(1000,700)
[ 1098.688456] input_size(1280,720), output_size(1000,700)
[ 1098.701628] mxc-isi 58130000.isi: mxc_isi_create_parition: can't alloc memory region for out_pending buffer[0]: -34

 

 

please help check it!

タグ(1)
0 件の賞賛
返信
9 返答(返信)

1,524件の閲覧回数
xu_ji1
Contributor V

hello,

what is progress now?

0 件の賞賛
返信

1,517件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please refer   L5.10.72_2.2.0_ISI_Workaround_for_ERR050145.zip in the knowledge base :

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-8X-B0-Linux-Reference-Patches-for-...

タグ(1)
0 件の賞賛
返信

1,515件の閲覧回数
xu_ji1
Contributor V

yes, I known it

for L5.10patch last update in Jan 4th until now this patch only for single camera use case

not apply multi camera use case. Both L5.10 and L5.4 patch missing multi camera use case protect

please update the patch like L4.14

0 件の賞賛
返信

1,489件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

If you are using multiple camera in L5.10 , you need also apply the 0002& 0003 patch in 4.14.98.

0 件の賞賛
返信

1,487件の閲覧回数
xu_ji1
Contributor V

I know it, but L4.14.98  0002&0003 patch not suitable for L5.10

there is many build error,please check it and provide patch for L5.10

0 件の賞賛
返信

1,542件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @xu_ji1 

Can you reproduce this on official BSP?

0 件の賞賛
返信

1,540件の閲覧回数
xu_ji1
Contributor V

Yes, we test on 8QXP MEK board with  L5.10.72 release reproduce the ISI overwrite issue

both single camera and multi camera cases can reproduced this issue,so we ask FAE and found the errata patch,but now add L5.10.72 patch with multi camera case also have issue

0 件の賞賛
返信

1,536件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @xu_ji1 

I found FAE still trace this issue, please refer their reply.

0 件の賞賛
返信

1,534件の閲覧回数
xu_ji1
Contributor V
ok,plz update if have solution
0 件の賞賛
返信