Processor Expert MQXLite component only works if KDS run as root (ubuntu)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Processor Expert MQXLite component only works if KDS run as root (ubuntu)

432 次查看
lopesjeronimo
Contributor I

I'm running KDS in Ubuntu (tested on 14.04, 14.10 and 15.05).

When I run KDS without root permissions (without sudo), and I add MQXLite component, I get this message:

"Warning: Selected version does not exist in directory \opt\Freescale\KDS_2.0.0\eclipse\ProcessorExpert\lib\mqxlite\. (MQX Lite version)"

If I run KDS with sudo, no problems.

Screenshot from 2015-04-10 08_53_37.png

0 项奖励
1 回复

302 次查看
marek_neuzil
NXP Employee
NXP Employee

Hello,

This known issue of Processor Expert that has been fixed in the upcoming release (it will be available soon). In KDS 2.0.0 you can use workaround that is described in the discussion thread Error using MQXlite from Linux

Best Regards,

Marek Neuzil

0 项奖励