I am running CW 10.5 Build 130916
I have generated SPI code for the K60DN512VMD10 chip (for SPI2)
In the attribute set list section, it will only accept 1 and 16 for both the HW input buffer size and the HW output buffer size.
This is incorrect (AFAICT), the values should be 1 or 4.
However, I am not sure this affects any of the generated code at all.
How important is this error?
已解决! 转到解答。
Hello,
I must confirm that this is really bug in latest version of PEx. However I think it should not influence code functionality. You can for example compare generated code when you set buffer size to 1 and to 16, the only difference is in DIS_TXF/DIS_RXF bitfields in MCR register. DIS_TXF/DIS_RXF bit-fields disable/enable FIFO -> size 4 or 16 should not influence driver functionality.
We will fix it for next release of PEx.
We are sorry for inconvenience.
Best regards
Vojtech Filip
Processor Expert Support Team
Hello,
I must confirm that this is really bug in latest version of PEx. However I think it should not influence code functionality. You can for example compare generated code when you set buffer size to 1 and to 16, the only difference is in DIS_TXF/DIS_RXF bitfields in MCR register. DIS_TXF/DIS_RXF bit-fields disable/enable FIFO -> size 4 or 16 should not influence driver functionality.
We will fix it for next release of PEx.
We are sorry for inconvenience.
Best regards
Vojtech Filip
Processor Expert Support Team