I created new project for Vybrid processor :
New Project -> Processor Expert Project ... -> Processors -> Vybrid -> MVF61NN151MK50 ... -> GNU C Compiler
Compiler reports error in the generated fiel Cpu.c
asm("mov r0,%0" : : "r" (&__vector_table));
^
../Generated_Code/Cpu.c:115:19: error: expected ')' before ':' token
asm("mov r0,%0" : : "r" (&__vector_table));
^
Robert
Solved! Go to Solution.
Hello Robert,
I have been able to reproduce the error with your project. I have verified the project settings and I have found out an incorrect settings of the C Compiler language standard. Please, select the GNU ISO C11(-std=gnu11) language standard to compile your application. See the screenshot below:
Please note, that this option affects support of the asm keyword, see details on the web page https://gcc.gnu.org/onlinedocs/gcc-4.5.2/gcc/C-Dialect-Options.html
Best Regards,
Marek Neuzil
Hello Robert,
I have created a project in PEx Driver Suite 10.4.2 and I have been able to build the application by using GNU C Compiler (I have used GNU C Compiler that is installed in KDS 3.0.0), see the console output below.
Could you provide me detail about the project you have created, please? (PEx Driver Suite version, operating system, CPU component settings, GNU C Compiler version, target compiler settings)
09:39:44 **** Incremental Build of configuration Debug for project Test MVF61NN151MK50 prj ****
make all
'Building file: ../Sources/Events.c'
'Invoking: Cross ARM C Compiler'
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O2 -Wall -g -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Generated_Code" -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Sources" -std=gnu11 -MMD -MP -MF"Sources/Events.d" -MT"Sources/Events.o" -c -o "Sources/Events.o" "../Sources/Events.c"
'Finished building: ../Sources/Events.c'
' '
'Building file: ../Sources/Exceptions.c'
'Invoking: Cross ARM C Compiler'
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O2 -Wall -g -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Generated_Code" -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Sources" -std=gnu11 -MMD -MP -MF"Sources/Exceptions.d" -MT"Sources/Exceptions.o" -c -o "Sources/Exceptions.o" "../Sources/Exceptions.c"
'Finished building: ../Sources/Exceptions.c'
' '
'Building file: ../Sources/main.c'
'Invoking: Cross ARM C Compiler'
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O2 -Wall -g -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Generated_Code" -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Sources" -std=gnu11 -MMD -MP -MF"Sources/main.d" -MT"Sources/main.o" -c -o "Sources/main.o" "../Sources/main.c"
'Finished building: ../Sources/main.c'
' '
'Building file: ../Project_Settings/Startup_Code/startupA5.asm'
'Invoking: Cross ARM GNU Assembler'
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O2 -Wall -g -x assembler-with-cpp -MMD -MP -MF"Project_Settings/Startup_Code/startupA5.d" -MT"Project_Settings/Startup_Code/startupA5.o" -c -o "Project_Settings/Startup_Code/startupA5.o" "../Project_Settings/Startup_Code/startupA5.asm"
'Finished building: ../Project_Settings/Startup_Code/startupA5.asm'
' '
'Building file: ../Generated_Code/Cpu.c'
'Invoking: Cross ARM C Compiler'
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O2 -Wall -g -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Generated_Code" -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Sources" -std=gnu11 -MMD -MP -MF"Generated_Code/Cpu.d" -MT"Generated_Code/Cpu.o" -c -o "Generated_Code/Cpu.o" "../Generated_Code/Cpu.c"
'Finished building: ../Generated_Code/Cpu.c'
' '
'Building file: ../Generated_Code/GIC.c'
'Invoking: Cross ARM C Compiler'
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O2 -Wall -g -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Generated_Code" -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Sources" -std=gnu11 -MMD -MP -MF"Generated_Code/GIC.d" -MT"Generated_Code/GIC.o" -c -o "Generated_Code/GIC.o" "../Generated_Code/GIC.c"
'Finished building: ../Generated_Code/GIC.c'
' '
'Building file: ../Generated_Code/MSCM.c'
'Invoking: Cross ARM C Compiler'
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O2 -Wall -g -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Generated_Code" -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Sources" -std=gnu11 -MMD -MP -MF"Generated_Code/MSCM.d" -MT"Generated_Code/MSCM.o" -c -o "Generated_Code/MSCM.o" "../Generated_Code/MSCM.c"
'Finished building: ../Generated_Code/MSCM.c'
' '
'Building file: ../Generated_Code/PE_LDD.c'
'Invoking: Cross ARM C Compiler'
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O2 -Wall -g -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Generated_Code" -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Sources" -std=gnu11 -MMD -MP -MF"Generated_Code/PE_LDD.d" -MT"Generated_Code/PE_LDD.o" -c -o "Generated_Code/PE_LDD.o" "../Generated_Code/PE_LDD.c"
'Finished building: ../Generated_Code/PE_LDD.c'
' '
'Building file: ../Generated_Code/Vectors.c'
'Invoking: Cross ARM C Compiler'
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O2 -Wall -g -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Generated_Code" -I"C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Sources" -std=gnu11 -MMD -MP -MF"Generated_Code/Vectors.d" -MT"Generated_Code/Vectors.o" -c -o "Generated_Code/Vectors.o" "../Generated_Code/Vectors.c"
'Finished building: ../Generated_Code/Vectors.c'
' '
'Building target: Test MVF61NN151MK50 prj.elf'
'Invoking: Cross ARM C++ Linker'
arm-none-eabi-g++ -mcpu=cortex-a5 -mthumb -O2 -Wall -g -T "C:/Freescale/KDS_3.0.0/workspace/Test MVF61NN151MK50 prj/Project_Settings/Linker_Files/ProcessorExpert.ld" -Xlinker --gc-sections -Wl,-Map,"Test MVF61NN151MK50 prj.map" -o "Test MVF61NN151MK50 prj.elf" ./Sources/Events.o ./Sources/Exceptions.o ./Sources/main.o ./Project_Settings/Startup_Code/startupA5.o ./Generated_Code/Cpu.o ./Generated_Code/GIC.o ./Generated_Code/MSCM.o ./Generated_Code/PE_LDD.o ./Generated_Code/Pins1.o ./Generated_Code/Vectors.o
'Finished building target: Test MVF61NN151MK50 prj.elf'
' '
09:39:48 Build Finished (took 4s.258ms)
Best Regards,
Marek Neuzil
Eclipse on MacOSX with GNU ARM plugin (no KDS!), Freescale Microcontrollers Driver Suite Plugin 10.4.2, GNU C 4.9.3 (Launchpad gcc-arm-none-eabi-4_9-2015q1) -> see attached screenshot of my eclipse plugin software. Second attachment is my Eclipse project.
Full build log with compiler switches (:
01:21:46 **** Build of configuration Debug for project TestVF61 ****
make all
Building file: ../Sources/Events.c
Invoking: Cross ARM C Compiler
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -I"/Users/Robert/Applications/EclipseCPP/ProcessorExpert/lib/Vybrid/iofiles" -I"/Users/Robert/Applications/EclipseCPP/ProcessorExpert/lib/Vybrid/pdd/inc" -I"/Users/Robert/Developer/Workspaces/EclipseCPP/TestVF61/Sources" -I"/Users/Robert/Developer/Workspaces/EclipseCPP/TestVF61/Generated_Code" -std=c99 -MMD -MP -MF"Sources/Events.d" -MT"Sources/Events.o" -c -o "Sources/Events.o" "../Sources/Events.c"
Finished building: ../Sources/Events.c
Building file: ../Sources/Exceptions.c
Invoking: Cross ARM C Compiler
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -I"/Users/Robert/Applications/EclipseCPP/ProcessorExpert/lib/Vybrid/iofiles" -I"/Users/Robert/Applications/EclipseCPP/ProcessorExpert/lib/Vybrid/pdd/inc" -I"/Users/Robert/Developer/Workspaces/EclipseCPP/TestVF61/Sources" -I"/Users/Robert/Developer/Workspaces/EclipseCPP/TestVF61/Generated_Code" -std=c99 -MMD -MP -MF"Sources/Exceptions.d" -MT"Sources/Exceptions.o" -c -o "Sources/Exceptions.o" "../Sources/Exceptions.c"
../Sources/Exceptions.c: In function 'Undefined_Handler':
../Sources/Exceptions.c:66:3: warning: implicit declaration of function 'asm' [-Wimplicit-function-declaration]
PE_DEBUGHALT();
^
Finished building: ../Sources/Exceptions.c
Building file: ../Sources/main.c
Invoking: Cross ARM C Compiler
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -I"/Users/Robert/Applications/EclipseCPP/ProcessorExpert/lib/Vybrid/iofiles" -I"/Users/Robert/Applications/EclipseCPP/ProcessorExpert/lib/Vybrid/pdd/inc" -I"/Users/Robert/Developer/Workspaces/EclipseCPP/TestVF61/Sources" -I"/Users/Robert/Developer/Workspaces/EclipseCPP/TestVF61/Generated_Code" -std=c99 -MMD -MP -MF"Sources/main.d" -MT"Sources/main.o" -c -o "Sources/main.o" "../Sources/main.c"
Finished building: ../Sources/main.c
Building file: ../Project_Settings/Startup_Code/startupA5.asm
Invoking: Cross ARM GNU Assembler
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -x assembler-with-cpp -MMD -MP -MF"Project_Settings/Startup_Code/startupA5.d" -MT"Project_Settings/Startup_Code/startupA5.o" -c -o "Project_Settings/Startup_Code/startupA5.o" "../Project_Settings/Startup_Code/startupA5.asm"
Finished building: ../Project_Settings/Startup_Code/startupA5.asm
Building file: ../Generated_Code/Cpu.c
Invoking: Cross ARM C Compiler
arm-none-eabi-gcc -mcpu=cortex-a5 -mthumb -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -g3 -I"/Users/Robert/Applications/EclipseCPP/ProcessorExpert/lib/Vybrid/iofiles" -I"/Users/Robert/Applications/EclipseCPP/ProcessorExpert/lib/Vybrid/pdd/inc" -I"/Users/Robert/Developer/Workspaces/EclipseCPP/TestVF61/Sources" -I"/Users/Robert/Developer/Workspaces/EclipseCPP/TestVF61/Generated_Code" -std=c99 -MMD -MP -MF"Generated_Code/Cpu.d" -MT"Generated_Code/Cpu.o" -c -o "Generated_Code/Cpu.o" "../Generated_Code/Cpu.c"
../Generated_Code/Cpu.c: In function '__init_hardware':
../Generated_Code/Cpu.c:115:3: warning: implicit declaration of function 'asm' [-Wimplicit-function-declaration]
asm("mov r0,%0" : : "r" (&__vector_table));
^
../Generated_Code/Cpu.c:115:19: error: expected ')' before ':' token
asm("mov r0,%0" : : "r" (&__vector_table));
^
make: *** [Generated_Code/Cpu.o] Error 1
01:21:47 Build Finished (took 1s.540ms)
BTW - KDS 3.0 was released? Does it support MacOSX?
Robert
Hello Robert,
I have been able to reproduce the error with your project. I have verified the project settings and I have found out an incorrect settings of the C Compiler language standard. Please, select the GNU ISO C11(-std=gnu11) language standard to compile your application. See the screenshot below:
Please note, that this option affects support of the asm keyword, see details on the web page https://gcc.gnu.org/onlinedocs/gcc-4.5.2/gcc/C-Dialect-Options.html
Best Regards,
Marek Neuzil
Yes, that's it. Thank you.