Code Warrior Ethernet Tap (PartNo: CWH-CTP-COP-YE) showing Connection Refused while programming flas

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior Ethernet Tap (PartNo: CWH-CTP-COP-YE) showing Connection Refused while programming flas

Jump to solution
1,459 Views
RAHULPADIGELLA
Contributor II

Sir,

We are using P1021 Power Quicc Processor for our application when we try to connect the CodeWarrior Ethernet Tap(P/N: CWH-CTP-COP-YE) an error is occured showing message as CCS ProtocolPlugin: CCS Connection Refused.

Kindly, if any one can help us in resolving this issue will be appreciated.cw.png

I have attached the snaps of the same.

0 Kudos
Reply
1 Solution
1,435 Views
Pavel
NXP Employee
NXP Employee
4 Replies
1,441 Views
RAHULPADIGELLA
Contributor II

Mr.Pavel,

We are using CW_ PA_v 8.8.5 Service Pack 1 for P1021  not CW_ PA_v 10.5.1 could you please suggest the solution for CW_ PA_v 8.8.5.

0 Kudos
Reply
1,447 Views
Pavel
NXP Employee
NXP Employee

Try to install CodeWarrior TAP driver again. See the ccs_drivers_installation_help.txt file for installing CodeWarrior TAP driver manually. This file is available using the following path:

C:\Freescale\CW_PA_v10.5.1\PA\ccs\drivers

 

See also the following file:

C:\Freescale\CW_PA_v10.5.1\PA\ccs\drivers\usb\readme.txt

 

Test your connection using the following commands in CCS window:

log v

source IDcode.tcl

0 Kudos
Reply
1,436 Views
Pavel
NXP Employee
NXP Employee

Install CodeWarrior 8.8.6 patch for using CodeWarrior TAP:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6121541

1,431 Views
RAHULPADIGELLA
Contributor II

Thank you Mr.Pavel , we have installed the CW 8.8.6 patch as you suggested.

The earlier issue CCS protocol plugin connection refused error is resolved. But we are facing new problem regarding Target Initialization. 

I have attached the snaps and P1021 Target Initialization code of the same for your reference.

Kindly, please help us to resolve this issue.

cwa.pngcwb.png

0 Kudos
Reply