MPC8541 Clocking Specific FAQs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8541 Clocking Specific FAQs

MPC8541 Clocking Specific FAQs

For MPC8541, what is the maximum bit rate clock for SSI? Is it really 12.285MHz or can it be run up to platform clock / 8?

Maximum bit rate clock for SSI is as per hardware spec i.e. 12.285MHz. This is the maximum speed at which the SSI IP is guaranteed to work.

From a system perspective it is possible to clock it at a higher speed, but for MPC8541 that is not supported.

If platform clock is 400MHz, please use appropriate values of DIV2, PSR and PM to ensure that the bit rate clock for SSI does not exceed 12.285MHz.


标签 (1)
无评分
版本历史
最后更新:
‎07-31-2012 10:47 AM
更新人: