bms displaying 0V for 4th battery when 4 battery cells are connected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bms displaying 0V for 4th battery when 4 battery cells are connected

1,626 Views
suvasis
Contributor I

hi,

I bought RDDRONE-BMS772 recently. Connected 4 cells, 3 cells display correct voltage but the 4th cell is displays 0v. Pls ref the images, can anyone point me to what else to do to correct this?

BMS display show cell 4 is 0V yellowBMS display show cell 4 is 0V yellow4th cell reading is good from here, 3.6V4th cell reading is good from here, 3.6V

 

0 Kudos
Reply
4 Replies

1,391 Views
suvasis
Contributor I

the reply helped.

0 Kudos
Reply

1,496 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can try to use 6s in this system to test again.

0 Kudos
Reply

1,466 Views
suvasis
Contributor I

1.The default is 3 and it is not auto detect..

2. they are working after I set the number of cells to 6.

Now it looks ok after the number of cells are set to 6.

0 Kudos
Reply

1,624 Views
suvasis
Contributor I

also attaching the configurations:

 

Screen Shot 2023-06-02 at 1.36.16 PM.pngScreen Shot 2023-06-02 at 1.36.22 PM.pngcell 3 reading is 3.6V and bms display also shows 3.6Vcell 3 reading is 3.6V and bms display also shows 3.6V

0 Kudos
Reply