bms displaying 0V for 4th battery when 4 battery cells are connected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bms displaying 0V for 4th battery when 4 battery cells are connected

2,540件の閲覧回数
suvasis
Contributor I

hi,

I bought RDDRONE-BMS772 recently. Connected 4 cells, 3 cells display correct voltage but the 4th cell is displays 0v. Pls ref the images, can anyone point me to what else to do to correct this?

BMS display show cell 4 is 0V yellowBMS display show cell 4 is 0V yellow4th cell reading is good from here, 3.6V4th cell reading is good from here, 3.6V

 

0 件の賞賛
返信
4 返答(返信)

2,305件の閲覧回数
suvasis
Contributor I

the reply helped.

0 件の賞賛
返信

2,410件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can try to use 6s in this system to test again.

0 件の賞賛
返信

2,380件の閲覧回数
suvasis
Contributor I

1.The default is 3 and it is not auto detect..

2. they are working after I set the number of cells to 6.

Now it looks ok after the number of cells are set to 6.

0 件の賞賛
返信

2,538件の閲覧回数
suvasis
Contributor I

also attaching the configurations:

 

Screen Shot 2023-06-02 at 1.36.16 PM.pngScreen Shot 2023-06-02 at 1.36.22 PM.pngcell 3 reading is 3.6V and bms display also shows 3.6Vcell 3 reading is 3.6V and bms display also shows 3.6V

0 件の賞賛
返信