FS26 unable to enter DFS State on KITFS26SKTEVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 unable to enter DFS State on KITFS26SKTEVM

470 Views
RChatterjee
Contributor III

On programming FS26 using KITFS26SKTEVM Rev E, it is programmed in emulation mode with the following configuration (using FS26 GUI FS26):

1. Wake1 Event triggers DFS Exit

2. DFS Enable is set to when FS0B or RSTB is asserted.

In this mode, when RSTB is held low, even after more than 30s, the FS26 is not entering DFS mode.

Can such a functionality be tested when running in emulation?

PFA images of said configuration

Labels (1)
0 Kudos
Reply
1 Reply

422 Views
guoweisun
NXP TechSupport
NXP TechSupport

 

Had replied based on case 00621526

 

0 Kudos
Reply