On programming FS26 using KITFS26SKTEVM Rev E, it is programmed in emulation mode with the following configuration (using FS26 GUI FS26):
1. Wake1 Event triggers DFS Exit
2. DFS Enable is set to when FS0B or RSTB is asserted.
In this mode, when RSTB is held low, even after more than 30s, the FS26 is not entering DFS mode.
Can such a functionality be tested when running in emulation?
PFA images of said configuration
Had replied based on case 00621526