FRDM-K82F Mounted But Won't Connect toNXP GUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K82F Mounted But Won't Connect toNXP GUI

1,151件の閲覧回数
swhite39
Contributor II

I have a KITVR5510DA0EVM, which is the VR5510 eval board. It utilizes the FRDM-K82F to faciliate communication between the PC running the NXP GUI and actually configuring the VR5510.

 

I followed the guide below (Section 5) to get the K82F updated.

https://www.nxp.com/docs/en/user-guide/UM11586.pdf

 

I was able to update the bootloader and application on the K82F, but I am having problems starting a session with the device through the NXP GUI. I can see the device is mounted through the file explorer on Windows 10, and right after I connect the device I do see the start session become "clickable", but then it immediately goes away and the light right next to J5 turns off on the K82F. This symptoms are repeatable by hot-plugging the USB cable. I have tried reflashing the K82F multiple times, no luck.

What should I try next?

0 件の賞賛
返信
1 返信

1,142件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Could you please share a short video of the procedure that you followed?

Regards,

David 

0 件の賞賛
返信