hello:
i want to run rapidIO message unit application on p4080ds,but it work failed,the follow is the log:
root@p4080ds:~# rmu
rmu: fsl_rmu_unit_uio_init(): /dev/rmu-uio-msg0: No such file or directory
rmu: main(): rmu_unit_uio_init(): No such file or directory
i use the rcw bin file that serdes config is 0x16 from SDK2.0, i use uImage-p4080ds-usdpaa.dtb file,and i use “0b01001100” on SW3 (Serdes reference clock for bank1 is 125MHz, bank2 is 125MHz, bank3 is 125MHz).
but i can't find the item is linux menucofing:
Device Drivers --->
<*> Userspace I/O drivers --->
<*> Freescale Rapidio Message Unit support
my sdk2.0 source code is 20160527 version
the uboot log is:
Warning: SERDES8 requires banks two and three to be disabled in the RCW
SRIO1: enabled but port error
SRIO2: enabled but port error
the kernel log is:
Setting up RapidIO peer-to-peer network /rapidio@ffe0c0000
fsl-of-rio ffe0c0000.rapidio: Of-device full name /rapidio@ffe0c0000
fsl-of-rio ffe0c0000.rapidio: Regs: [mem 0xffe0c0000-0xffe0d0fff]
fsl-of-rio ffe0c0000.rapidio: bellirq: 57
fsl-of-rio ffe0c0000.rapidio: pwirq: 478
fsl-of-rio ffe0c0000.rapidio: /rapidio@ffe0c0000/port1: LAW start 0x0000000c20000000, size 0x0000000010000000.
fsl-of-rio ffe0c0000.rapidio: RapidIO PHY type: Serial
fsl-of-rio ffe0c0000.rapidio: Port 0 is not ready. Try to restart connection...
fsl-of-rio ffe0c0000.rapidio: Port 0 restart failed.
fsl-of-rio ffe0c0000.rapidio: /rapidio@ffe0c0000/port2: LAW start 0x0000000c30000000, size 0x0000000010000000.
fsl-of-rio ffe0c0000.rapidio: RapidIO PHY type: Serial
fsl-of-rio ffe0c0000.rapidio: Port 1 is not ready. Try to restart connection...
fsl-of-rio ffe0c0000.rapidio: Port 1 restart failed.
fsl-of-rio: probe of ffe0c0000.rapidio failed with error -67
please help me,thank you
You wrote:
> i can't find the item is linux menucofing
What do you see in the:
Device Drivers --->
<*> Userspace I/O drivers --->
?
Assuming that the SDK was not installed properly the latest SDK version can be downloaded from:
Linux® SDK for QorIQ® Processors | NXP
Detailed description of the RMU testing on P4080DS is provided in the SDK Documentation:
You wrote:
> is that need a special ucode for Fman?
Microcode is required for FMan, but FMan operation is not connected with RapidIO.
thanks for your reply
<*> Userspace I/O drivers ---> is the follow:
i use sdk2.0 20160527 version download from Linux® SDK for QorIQ® Processors | NXP ,because SDK2.0 version 2017.3 can't be compiled due to www.freescale.com is shut down
the method of download sdk2.0 20160527 is supplied by wang yiping,another NXP FAE
is that need a special ucode for Fman? i use fsl_fman_ucode_p4080_r3.0_106_2_18.bin file for fman