P2020 how much FLOPS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 how much FLOPS

1,037 Views
smiletan
Contributor I

I am ready to use P2020.My application want strong float point processing capacity  bigger than 13GPLOPS.Is the chip P2020 OK for my app?

0 Kudos
Reply
2 Replies

975 Views
smiletan
Contributor I

Thanks.

Then IMX6Q float point processing capacity ? Can I use IMX6Q to suit for 13GFLOPS?

0 Kudos
Reply

975 Views
ufedor
NXP Employee
NXP Employee

> My application want strong float point processing capacity bigger than 13GPLOPS.

> Is the chip P2020 OK for my app?

No.

P2020 has e500v2 cores executing floating-point arithmetic instructions, except for divide, with 1-cycle throughput.

For two cores at 1333 MHz this could give 2.6 GFLOPs

0 Kudos
Reply