What are the DMIPS/MHz and GFLOP number of P5010/ 20 processors ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What are the DMIPS/MHz and GFLOP number of P5010/ 20 processors ?

跳至解决方案
1,388 次查看
doner_t
Contributor II

Hello,

  • I need to DMIPS/MHz and GFLOP number of e5500 core. Could you help me ?
  • Another question is that does e5500 core provide ECC on its L1 cache ?

Best Regards,

Tugay

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
753 次查看
ufedor
NXP Employee
NXP Employee

1) 3.0 DMIPS/MHz

2) ECC is not implemented.

The L1 caches have:

— Instruction cache: 1 parity bit per word of instruction, 1 bit of parity per tag

— Data cache: 1 parity bit per byte of data, 1 bit of parity per tag

在原帖中查看解决方案

0 项奖励
回复
1 回复
754 次查看
ufedor
NXP Employee
NXP Employee

1) 3.0 DMIPS/MHz

2) ECC is not implemented.

The L1 caches have:

— Instruction cache: 1 parity bit per word of instruction, 1 bit of parity per tag

— Data cache: 1 parity bit per byte of data, 1 bit of parity per tag

0 项奖励
回复