Hello to all,
I'm working on P2041RDB board and I'm trying PXE boot. for that i configured the u-boot variables ipaddr, ethaddr, netmask, gatewayip, ethact .
and i ran the ping command but i'm getting error like as follows..........
=> ping 192.168.2.144
FM1@DTSEC1: No link.
FM1@DTSEC2: No link.
FM1@DTSEC3: No link.
FM1@DTSEC4: No link.
FM1@DTSEC5: No link.
ping failed; host 192.168.2.144 is not alive
..........What are the reasons to get that error message.... and this is the total console out put is as follows ...............
U-Boot 2011.12-00064-gbfb0c9a (Jun 15 2012 - 18:21:35)
CPU0: P2041E, Version: 1.1, (0x82180111)
Core: E500MC, Version: 2.2, (0x80230022)
Clock Configuration:
CPU0:1500 MHz, CPU1:1500 MHz, CPU2:1500 MHz, CPU3:1500 MHz,
CCB:750 MHz,
DDR:666.667 MHz (1333.333 MT/s data rate) (Asynchronous), LBC:93.750 MHz
FMAN1: 583.333 MHz
PME: 375 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P2041RDB, CPLD version: 4.0 vBank: 0
36-bit Addressing
Reset Configuration Word (RCW):
00000000: 12600000 00000000 241c0000 00000000
00000010: 648ea0c1 c3c02000 de800000 40000000
00000020: 00000000 00000000 00000000 d0030f07
00000030: 00000000 00000000 00000000 00000000
SERDES Reference Clocks: Bank1=100Mhz Bank2=125Mhz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM UG51U6400N8SU-ACF
2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=9, ECC off)
DDR Chip-Select Interleaving Mode: CS0+CS1
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
Flash: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 1024 KB enabled
SERDES: bank 3 disabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_SDHC: 0
EEPROM: Invalid ID (ff ff ff ff)
PCIe1: disabled
PCIe2: Root Complex, no link, regs @ 0xfe201000
PCIe2: Bus 00 - 00
PCIe3: disabled
In: serial
Out: serial
Err: serial
Net: Initializing Fman
Fman1: Uploading microcode version 106.1.4
FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5
Hit any key to stop autoboot: 0
=>
=> pri ipaddr
ipaddr=192.168.2.168
=> pri etha
ethact ethaddr
=> pri ethaddr
ethaddr=00-04-9F-02-4C-4C
=> printenv netmask
netmask=255.255.255.0
=> printenv gatewayip
gatewayip=192.168.2.123
=> printenv ethact
ethact=FM1@DTSEC1
=> ping 192.168.2.144
FM1@DTSEC1: No link.
FM1@DTSEC2: No link.
FM1@DTSEC3: No link.
FM1@DTSEC4: No link.
FM1@DTSEC5: No link.
ping failed; host 192.168.2.144 is not alive
=>
Original Attachment has been moved to: ping_issue.log.zip
Hi! Im working embedding U-Boot on a raspberry pi 3b and i have the same issue.
But look what i have discovered. If you ping from the PC to the Raspberry it fails, but if you ping from U-Boot to the PC it will success and you will be able to reach the PC. The most surprising thing is that the pc ping start functioning while the raspberry is pinging the host.
I dont have time to investigate this, but if you only are looking for checking u-boot network connection as i am, this will be useful.
Hi all,
Any news about this issue? I have the same problem with the P3041.
Some simple initial tips:
1. Make sure the cable is correctly connected to the right ethernet port on the board (there are several ports)
2. Make sure the host 192.168.2.144 is normally available, you may use a third host to ping to the 192.168.2.144.
3. Check the switch settings whether they are all in default postion as the board quick start document.
Hilunminliang,
Thanks for you kind reply....
I've ensured the switch settings. all are in default... and the cable is also connected to the right ports(one to one)..
Even If i didn't connect any Ethernet cable. It should take some time to ping and display failed message. But it is not happening like that.
it's directly showing "No link." message with in a fraction of seconds. what would be the reason.....
Thanks,
Rajasekhar
Please provide additional U-Boot logs:
1) of the "pri" command
2) of the "mdio list" command
3) to which exactly socket the Ethernet cabe is connected?
Please also ensure all the on board jumpers are in default position (Refer to the board quick start guide)
U-Boot 2011.12-00064-gbfb0c9a (Jun 15 2012 - 18:21:35)
CPU0: P2041E, Version: 1.1, (0x82180111)
Core: E500MC, Version: 2.2, (0x80230022)
Clock Configuration:
CPU0:1500 MHz, CPU1:1500 MHz, CPU2:1500 MHz, CPU3:1500 MHz,
CCB:750 MHz,
DDR:666.667 MHz (1333.333 MT/s data rate) (Asynchronous), LBC:93.750 MHz
FMAN1: 583.333 MHz
PME: 375 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P2041RDB, CPLD version: 4.0 vBank: 0
36-bit Addressing
Reset Configuration Word (RCW):
00000000: 12600000 00000000 241c0000 00000000
00000010: 648ea0c1 c3c02000 de800000 40000000
00000020: 00000000 00000000 00000000 d0030f07
00000030: 00000000 00000000 00000000 00000000
SERDES Reference Clocks: Bank1=100Mhz Bank2=125Mhz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM UG51U6400N8SU-ACF
2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=9, ECC off)
DDR Chip-Select Interleaving Mode: CS0+CS1
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
Flash: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 1024 KB enabled
SERDES: bank 3 disabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_SDHC: 0
EEPROM: Invalid ID (ff ff ff ff)
PCIe1: disabled
PCIe2: Root Complex, no link, regs @ 0xfe201000
PCIe2: Bus 00 - 00
PCIe3: disabled
In: serial
Out: serial
Err: serial
Net: Initializing Fman
Fman1: Uploading microcode version 106.1.4
FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5
Hit any key to stop autoboot: 3
=>
=> pri
baudrate=115200
bdev=sda3
bootcmd=run sataboot
bootdelay=3
bootfile=uImage-p2041rdb.bin
consoledev=ttyS0
defaultboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;bootm e8020000 e9300000 e8800000
eth1addr=00-04-9F-02-4C-4D
eth2addr=00-04-9F-02-4C-4E
eth3addr=00-04-9F-02-4C-4F
eth4addr=00-04-9F-02-4C-50
eth5addr=00-04-9F-02-4C-51
eth6addr=00:E0:0C:00:ea:06
eth7addr=00:E0:0C:00:ea:07
eth8addr=00:E0:0C:00:ea:08
eth9addr=00:E0:0C:00:ea:09
ethact=FM1@DTSEC1
ethaddr=00-04-9F-02-4C-4C
ethprime=e1000#0
fdtaddr=c00000
fdtfile=uImage-p2041rdb.dtb
filesize=80000
fman_ucode=0xef000000
gatewayip=192.168.2.123
hvboot=setenv bootargs config-addr=0xfe8900000;bootm 0xfe8700000 - 0xfe8800000
hwconfig=fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1;fsl_fm1_xaui_phy:xfi
ipaddr=192.168.2.158
loadaddr=1000000
netdev=eth0
netmask=255.255.255.0
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr - $fdtaddr
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr
ramdiskaddr=2000000
ramdiskfile=devel-image-p2041rdb.ext2.gz.u-boot
rootpath=/opt/nfsroot
sataboot=setenv bootargs root=/dev/sda3 rw rootdelay=5 console=$consoledev,$baudrate $othbootargs;bootm e8020000 - e8800000
serverip=192.168.2.144
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ubootaddr +$filesize && cmp.b $loadaddr $ubootaddr $filesize
uboot=u-boot.bin
ubootaddr=0xeff80000
usbboot=setenv bootargs root=/dev/sdb1 rw rootdelay=10 console=ttyS0,115200; bootm 0xe8020000 - e8800000
Environment size: 2043/8188 bytes
=>
=>
=>
=> mdio list
FSL_MDIO0:
0 - Generic PHY <--> FM1@DTSEC5
1 - Generic PHY <--> FM1@DTSEC4
2 - Generic PHY <--> FM1@DTSEC1
3 - Generic PHY <--> FM1@DTSEC2
4 - Generic PHY <--> FM1@DTSEC3
FM_TGEC_MDIO:
=>
=> ping 192.168.2.144
FM1@DTSEC1: No link.
FM1@DTSEC2: No link.
FM1@DTSEC3: No link.
FM1@DTSEC4: No link.
FM1@DTSEC5: No link.
ping failed; host 192.168.2.144 is not alive
=>
=>
The RDB team compared the log file with the quick start guide(see attached).
Uboot revision should be same, but Fman code revision and rcw are different.
Please try attached rcw and ucode.
If still not work, maybe hardware issue somewhere.
Is the board brand new?
Hi LunMinLiang,
I was also facing similar issue with my P4080DS board while trying to update with SDK 1.7 images, after this error, I cannot connect to any interface to download my images not even from tftp.
Please find my u-boot log details:
U-Boot 2014.07QorIQ-SDK-V1.7+g659b6a2 (Feb 27 2015 - 08:30:18)
CPU0: P4080E, Version: 3.0, (0x82080030)
Core: e500mc, Version: 3.1, (0x80230031)
Clock Configuration:
CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz, CPU3:1499.985 MHz,
CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz, CPU7:1499.985 MHz,
CCB:799.992 MHz,
DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999 MHz
FMAN1: 599.994 MHz
FMAN2: 599.994 MHz
QMAN: 399.996 MHz
PME: 399.996 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 105a0000 00000000 1e1e181e 0000cccc
00000010: 40464000 3c3c2000 fe800000 61000000
00000020: 00000000 00000000 00000000 008b6000
00000030: 00000000 00000000 00000000 00000000
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM i-DIMM
Detected UDIMM i-DIMM
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR
4 GiB (DDR3, 64-bit, CL=9, ECC on)
DDR Controller Interleaving Mode: cache line
DDR Chip-Select Interleaving Mode: CS0+CS1
POST memory PASSED
Flash: 128 MiB
L2: 128 KiB enabled
Corenet Platform Cache: 2 MiB enabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_SDHC: 0
EEPROM: CRC mismatch (ba9a52e2 != ffffffff)
PCIe1: Root Complex, no link, regs @ 0xfe200000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, x1 gen1, regs @ 0xfe202000
02:00.0 - 1095:3132 - Mass storage controller
PCIe3: Bus 01 - 02
In: serial
Out: serial
Err: serial
Net: Fman1: Data at eff00000 is not a firmware
No ethernet found.
Hit any key to stop autoboot: 0
=> mdio list
FSL_MDIO0:
FM_TGEC_MDIO:
P4080DS_MDIO0:
P4080DS_MDIO8:
P4080DS_MDIO4:
P4080DS_MDIO12:
P4080DS_MDIO1:
P4080DS_MDIO3:
=> pri
baudrate=115200
bdev=sda3
bootcmd=setenv bootargs root=/dev/$bdev rw console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr - $fdtaddr
bootdelay=10
bootfile=uImage
consoledev=ttyS0
eth1addr=00:04:9F:03:56:DE
eth2addr=00:04:9F:03:56:DF
eth3addr=00:04:9F:03:56:E0
eth4addr=00:04:9F:03:56:E1
eth5addr=00:04:9F:03:56:E2
eth6addr=00:04:9F:03:56:E3
eth7addr=00:04:9F:03:56:E4
eth8addr=00:04:9F:03:56:E5
eth9addr=00:04:9F:03:56:E6
ethact=FM1@DTSEC2
ethaddr=00:04:9F:03:56:DD
ethprime=FM1@DTSEC2
fdtaddr=c00000
fdtfile=p4080ds/p4080ds.dtb
hwconfig=fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1;usb1:dr_mode=host,phy_type=ulpi;usb2:dr_mode=peripheral,phy_type=ulpi
ipaddr=10.10.10.148
loadaddr=1000000
netdev=eth0
netmask=255.255.255.0
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr - $fdtaddr
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr
ramdiskaddr=2000000
ramdiskfile=p4080ds/ramdisk.uboot
rootpath=/opt/nfsroot
serverip=10.10.10.155
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ubootaddr +$filesize && cmp.b $loadaddr $ubootaddr $filesize
uboot=u-boot.bin
ubootaddr=0xeff40000
Environment size: 1703/8188 bytes
=>
Could you please suggest anything that could I try as I messed up the alternate bank also with this?
Thanks,
Sharath Chandra
Hi Sharath Chandra,
Do you mean ping works normal before you update to SDK 1.7?
Can you please try the available pre-built image provided in SDK 1.7?
Have a great day,
Lunmin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Lumin,
Yes, ping used to work. After I update with u-boot, it looks like the memory layout has changed and it was not able to find the microcode in its address.
After flashing the microcode by hardware debugger to that required address,it is working fine now.
Thanks for help,
Sharath Chandra
Hi Sharath Chandra,
Welcome. So ping works fine on fm1-gb1, with the pre-built image in SDK1.7?
But you still see the message in below post?
DPFM1 - invalid FM Controller action code: 54360
Have a great day,
Lunmin
Hi Lumin,
Ping works fine.
Just the kernel image is different from pre-built binaries of SDK 1.7.
The difference is that I rebuilt the kernel with Timer Interrupt Frequency set to 1000Hz( the default is 250 Hz).
and I used this image for the kernel.
Does this affect anything?
Thanks,
Sharath Chandra
Hi,
I am facing similar issue in P2041RDB. Please let me know how to re-flash the u-code? we are using lauterbach for debugging if you have any reference script to flash u-code please share.
Thanks and Regards,
Veerendranath
LunMinLiang,
I have the same issue. I have provided my U-Boot. I believe that my ucode & rcw are updated (current rev 2 board). Please help.
-Robert Davis
U-Boot 2013.01QorIQ-SDK-V1.5 (Dec 15 2013 - 18:54:15)
CPU0: T4240E, Version: 2.0, (0x82480020)
Core: E6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1666.667 MHz, CPU1:1666.667 MHz, CPU2:1666.667 MHz, CPU3:1666.667 MHz,
CPU4:1666.667 MHz, CPU5:1666.667 MHz, CPU6:1666.667 MHz, CPU7:1666.667 MHz,
CPU8:1666.667 MHz, CPU9:1666.667 MHz, CPU10:1666.667 MHz, CPU11:1666.667 MHz,
CCB:733.333 MHz,
DDR:933.333 MHz (1866.667 MT/s data rate) (Asynchronous), IFC:183.333 MHz
FMAN1: 733.333 MHz
FMAN2: 733.333 MHz
QMAN: 366.667 MHz
PME: 533.333 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Reset Configuration Word (RCW):
00000000: 16070019 18101916 00000000 00000000
00000010: 04383060 30548c00 ec020000 f5000000
00000020: 00000000 ee0000ee 00000000 000307fc
00000030: 00000000 00000000 00000000 00000028
Board: T4240QDS, Sys ID: 0x1e, Sys Ver: 0x14, vBank: 0
FPGA: v6 (T4240QDS_2014_0211_1852), build 547 on Wed Feb 12 00:52:40 2014
SERDES Reference Clocks: SERDES1=125MHz SERDES2=125MHz SERDES3=100MHz SERDES4=100MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM
Detected UDIMM
Detected UDIMM
22 GiB left unmapped
DDR: 24 GiB (DDR3, 64-bit, CL=13, ECC on)
DDR Controller Interleaving Mode: 3-way 4KB
DDR Chip-Select Interleaving Mode: CS0+CS1
VID: Core voltage 1030 mV
Flash: 128 MiB
L2: 2048 KB enabled
enable l2 for cluster 1 fec60000
enable l2 for cluster 2 feca0000
Corenet Platform Cache: 1536 KB enabled
Using SERDES1 Protocol: 1 (0x1)
Using SERDES2 Protocol: 28 (0x1c)
Using SERDES3 Protocol: 6 (0x6)
Using SERDES4 Protocol: 12 (0xc)
SRIO1: enabled
SRIO2: disabled
NAND: 512 MiB
MMC: FSL_SDHC: 0
EEPROM: CRC mismatch (11919b47 != 00000000)
PCIe1: Root Complex, no link, regs @ 0xfe240000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, no link, regs @ 0xfe260000
PCIe3: Bus 01 - 01
PCIe4: disabled
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 106.4.10
Failed to connect
Failed to connect
Fman2: Uploading microcode version 106.4.10
FM1@DTSEC5 [PRIME], FM2@DTSEC5
Hit any key to stop autoboot: 0
=> pri ipaddr
ipaddr=192.168.0.2
ipaddr=10.11.192.53
baudrate=115200
bdev=sda3
bootargs=root=/dev/ram rw console=ttyS0,115200
bootcmd=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;bootm e8020000 e9300000 e8800000
bootdelay=10
bootfile=uImage
c=ffe
consoledev=ttyS0
eth0addr=00:04:9f:03:67:4a
eth10addr=00:04:9f:03:67:54
eth11addr=00:04:9f:03:67:55
eth12addr=00:04:9f:03:67:56
eth13addr=00:04:9f:03:67:57
eth14addr=00:04:9f:03:67:58
eth15addr=00:04:9f:03:67:59
eth1addr=00:04:9f:03:67:4b
eth2addr=00:04:9f:03:67:4c
eth3addr=00:04:9f:03:67:4d
eth4addr=00:04:9f:03:67:4e
eth5addr=00:04:9f:03:67:4f
eth6addr=00:04:9f:03:67:50
eth7addr=00:04:9f:03:67:51
eth8addr=00:04:9f:03:67:52
eth9addr=00:04:9f:03:67:53
ethact=FM1@DTSEC5
ethaddr=00:04:9f:03:67:4a
ethprime=FM1@DTSEC5
fdtaddr=c00000
fdtfile=t4240qds/t4240qds.dtb
fileaddr=1000000
filesize=200000
fman_ucode=0xeff40000
gatewayip=10.11.192.1
hwconfig=fsl_ddr:ctlr_intlv=3way_4KB,bank_intlv=auto;usb1:dr_mode=host,phy_type=utmi
ipaddr=192.168.0.2
loadaddr=1000000
netdev=eth0
netmask=255.255.248.0
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr - $fdtaddr
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr
ramdiskaddr=2000000
ramdiskfile=t4240qds/ramdisk.uboot
rootpath=/opt/nfsroot
sataboot=setenv bootargs root=/dev/sda1 rootdelay=5 rw console=$consoledev,$baudrate $othbootargs;bootm e8020000 - e8800000
serverip=10.11.199.103
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ubootaddr +$filesize && cmp.b $loadaddr $ubootaddr $filesize
uboot="u-boot.bin"
ubootaddr=0xeff80000
Environment size: 2123/8188 bytes
=> ping 10.11.199.103
Using FM1@DTSEC5 device
ping failed; host 10.11.199.103 is not alive