P4080 rcw file unknown register address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P4080 rcw file unknown register address

ソリューションへジャンプ
1,153件の閲覧回数
gaolixing
Contributor I

hello, i am reading rcw file rcw_2sgmii_1500mhz_rev3.bin for p4080ds,in the PBI command segment, 89 0B 00 64 00 00 00 02 command is write 00 00 00 02 value to register address 0B 00 64 in altnative configuration space,but i can't find the register address 0B 00 64 in the p4080ds reference manual,where can i find these registers definition address at 0B 00 64,0B 00 60 and so on.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,104件の閲覧回数
ufedor
NXP Employee
NXP Employee

The PBI command in question is needed to implement an erratum workaround.

Please create Technical Case if additional information is needed because it is confidential:

https://support.nxp.com/ 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,105件の閲覧回数
ufedor
NXP Employee
NXP Employee

The PBI command in question is needed to implement an erratum workaround.

Please create Technical Case if additional information is needed because it is confidential:

https://support.nxp.com/ 

0 件の賞賛
返信