P4080 rcw file unknown register address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

P4080 rcw file unknown register address

跳至解决方案
1,505 次查看
gaolixing
Contributor I

hello, i am reading rcw file rcw_2sgmii_1500mhz_rev3.bin for p4080ds,in the PBI command segment, 89 0B 00 64 00 00 00 02 command is write 00 00 00 02 value to register address 0B 00 64 in altnative configuration space,but i can't find the register address 0B 00 64 in the p4080ds reference manual,where can i find these registers definition address at 0B 00 64,0B 00 60 and so on.

标签 (1)
0 项奖励
回复
1 解答
1,456 次查看
ufedor
NXP Employee
NXP Employee

The PBI command in question is needed to implement an erratum workaround.

Please create Technical Case if additional information is needed because it is confidential:

https://support.nxp.com/ 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,457 次查看
ufedor
NXP Employee
NXP Employee

The PBI command in question is needed to implement an erratum workaround.

Please create Technical Case if additional information is needed because it is confidential:

https://support.nxp.com/ 

0 项奖励
回复