P4080 rcw file unknown register address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080 rcw file unknown register address

Jump to solution
1,148 Views
gaolixing
Contributor I

hello, i am reading rcw file rcw_2sgmii_1500mhz_rev3.bin for p4080ds,in the PBI command segment, 89 0B 00 64 00 00 00 02 command is write 00 00 00 02 value to register address 0B 00 64 in altnative configuration space,but i can't find the register address 0B 00 64 in the p4080ds reference manual,where can i find these registers definition address at 0B 00 64,0B 00 60 and so on.

Labels (1)
0 Kudos
Reply
1 Solution
1,099 Views
ufedor
NXP Employee
NXP Employee

The PBI command in question is needed to implement an erratum workaround.

Please create Technical Case if additional information is needed because it is confidential:

https://support.nxp.com/ 

View solution in original post

0 Kudos
Reply
1 Reply
1,100 Views
ufedor
NXP Employee
NXP Employee

The PBI command in question is needed to implement an erratum workaround.

Please create Technical Case if additional information is needed because it is confidential:

https://support.nxp.com/ 

0 Kudos
Reply