Looks like the open source world is working on a solution:
http://www.mono-project.com/docs/about-mono/
.NET Framework Class Library - The Mono platform provides a comprehensive set of classes that provide a solid foundation to build applications on. These classes are compatible with Microsoft’s .Net Framework classes.
Looks like the open source world is working on a solution:
http://www.mono-project.com/docs/about-mono/
.NET Framework Class Library - The Mono platform provides a comprehensive set of classes that provide a solid foundation to build applications on. These classes are compatible with Microsoft’s .Net Framework classes.
Sorry, we are unaware about any tools to run Windows or .NET applications to run on Power architecture.
I see .NET is available for several Linux distributions, still only x86/x64 architecture is supported.
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------