Hi All,
I'm using the evaluation board of S32R41,trying to integrate the tcp/ip stack (lwip)。Refering to NXP's demo "lwip_S32R41_NXP_RTOS_M7_0",I configure GMAC and lwip stack on core M7_1 in another demo project called "S32R41+TEF82xx_Development_Platform"。However,the result is not as expected,failure for ping。The code get stuck in the function "gmacif_low_level_output",and GMAC TX/RX interrupt handdle can not be triggered。I have no idea what needs to be concerned,anyone can help with it ?
Hello,
unfortunately the RADAR application support is limited and the team is not answering on communities.
This looks like application issue. Could you submit the ticket at NXP.com so your question will reach the team.
Best regards,
Peter