sja1105 traffic Forwarding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sja1105 traffic Forwarding

1,089件の閲覧回数
haiyang
Contributor III

hi,

i use sja1105 to designe a switch ;

I want to implement a traffic forwarding function, all the traffic from port0 forwarding to port3,

What configuration should I do?

And i dont want  use vLAN ,is there a simple mirror function? 

best wish

タグ(1)
0 件の賞賛
返信
1 返信

1,069件の閲覧回数
kaden
NXP Employee
NXP Employee

Hi @haiyang ,

i do have a few questions to provide an appropriate answer.

Which variant are you using? SJA1105PQRS or the older SJA1105TEL? We recommend using the SJA1105PQRS for new designs.

Which tools are you currently using to generate a configuration for the device? 

BR

Kevin  

 

0 件の賞賛
返信