#MC33908 - Hello, I am curious what continuous reverse polarity the MC33908 #Vsense pin can withstand. My implementation includes the external 5.1kOhm resistor, but the maximum ratings only show -14.0V as the max rating, no clamping voltage or current that the pin can withstand. If a current were provided I could calculate. There are also resistive dividers internal to the MC33908 on the Vsense pin, but the values of these are not given, again with the values of these, the -14V could be extrapolated to the input voltage with the 5.1k resistor.
Any help you can provide would be appreciated,
Thanks,
Josh