ls1012A quad enable bit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1012A quad enable bit

1,260 次查看
yogeshddave
Contributor II

Dear All,

I am using LS1012A-FRWY and it has Winbond SPI flash. I want to set quad-enable bit (QE bit) of status register2 to 1. can somebody guide how to achieve this?

I also want to know which QE bit number of status register 2 is applicable for winbond like devices. Moreover it will be helpful if someone knows If there is any way to check the status of this Quad Enable bit?

Thanks in advance.!

0 项奖励
回复
1 回复

1,173 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following update from the AE team.

This information should be available in the Winbond SPI flash datasheet/manual. Customers can use similar steps to those used for writing on the flash. However, to write to the flash internal registers, the opcode for the command will be different (which should be available in the flash documents).

0 项奖励
回复