iMX27 GPIO access

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX27 GPIO access

3,229件の閲覧回数
quentin
Contributor I

Hi,

 

I would like to access some gpio (some in input, other in output) in a program to use with Led and button.

The code below seems to work but as no effect on the led itself (even if the DR is effectively change)

 

May be I m not using the good offset in mmap (GPIO_BASE ?) at first I use 0x10015000 but after some search in the kernel source I tried with the virtual address 0xf4015000.

 

PS: I checked the different value of DDIR (out), GIUS (inuse) and GPR and all seems fine.

 

I would really appreciate some help here :smileyhappy:

 

#include <stdlib.h>#include <stdio.h>#include <fcntl.h>#include <sys/mman.h>#include <linux/fb.h>#include <unistd.h>#include <stropts.h>#include <errno.h>unsigned long *memregs32;int memfd;#define GPIO_BASE 0xf4015000//#define GPIO_BASE 0x10015000void *trymmap (void *start, size_t length, int prot, int flags, int fd, off_t offset){ char *p; int aa; printf ("mmap(%X, %X, %X, %X, %X, %X) ... ", (unsigned int)start, length, prot, flags, fd, (unsigned int)offset); p = mmap (start, length, prot, flags, fd, offset); if (p == (char *)0xFFFFFFFF) { aa = errno;  printf ("failed. errno = %d\n", aa); }else { printf ("OK! (%X)\n", (unsigned int)p); } return p;}unsigned char initphys (void){ memfd = open("/dev/mem", O_RDWR); if (memfd == -1) { printf ("Open failed\n");  return 0; } printf ("/dev/mem opened successfully - fd = %d\n", memfd); memregs32 = trymmap(0, 0x10000, PROT_READ|PROT_WRITE, MAP_SHARED, memfd, GPIO_BASE); if (memregs32 == (unsigned long *)0xFFFFFFFF) return 0; return 1;}void closephys (void){ close (memfd);}int main(void){ int i; if (!initphys()) return 0; printf ("Reading GPIO pins...\n"); printf ("DDIR = %08X\n", memregs32[0x400]); printf ("OCR1 = %08X\n", memregs32[0x404]); printf ("OCR2 = %08X\n", memregs32[0x408]); memregs32[0x408] |= 0x300; printf ("OCR2 = %08X\n", memregs32[0x408]); printf ("ICONFA1 = %08X\n", memregs32[0x40C]); printf ("ICONFA2 = %08X\n", memregs32[0x410]); printf ("ICONFB1 = %08X\n", memregs32[0x414]); printf ("ICONFB2 = %08X\n", memregs32[0x418]); printf ("DR = %08X\n", memregs32[0x41C]); printf ("GIUS = %08X\n", memregs32[0x420]); printf ("SSR = %08X\n", memregs32[0x424]); printf ("ICR1 = %08X\n", memregs32[0x428]); printf ("ICR2 = %08X\n", memregs32[0x42C]); printf ("IMR = %08X\n", memregs32[0x430]); printf ("ISR = %08X\n", memregs32[0x434]); printf ("GPR = %08X\n", memregs32[0x438]); printf ("SWR = %08X\n", memregs32[0x43C]); printf ("PUEN = %08X\n", memregs32[0x440]);  printf ("Flash battery LED...\n"); for (i = 0; i < 9; i ++) { memregs32[0x41C] ^= 0x00100000;  printf ("%s\n", memregs32[0x41C] & 0x00100000 ? "on" : "off"); } closephys(); printf("test complete\n"); return 0;}

 

 

 

0 件の賞賛
返信
3 返答(返信)

1,704件の閲覧回数
andreas_b
Contributor I

It should be the physical address as GPIO_BASE, i.e. 0x10015000

The problem seems to be that since the pointer *memregs32 is of type long every address from GPIO_BASE will actually be 4 bytes.

Therefore every address accessed using memregs32 should be divided by 4, something like:

...memregs32[0x400/4]...

 

 

I think... :smileyhappy:

 

0 件の賞賛
返信

1,704件の閲覧回数
andreas_b
Contributor I

Hi,

I'm facing the same kind of problem. Trying to draw a gpio-signal first low and then high but no matter what I attempt it doesn't work. No action at all while measuring with an oscilloscope so if you have come up with something new I would really appreciate if you could share it :smileyhappy:

 

(Or if someone else has some info?!)

 

Br,

Andreas

0 件の賞賛
返信

1,704件の閲覧回数
quentin
Contributor I

Well for now I use the sysfs interface to read my gpio but when I try to change the value of an output gpio, the change doesn't take effect even if no error is return.So I m stuck there.

 

here an example : http://docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:gpio-sysfs

 

 

It would be nice to know the gpio base address to use with mmap for the imx27.

0 件の賞賛
返信