guides l for Box Label

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

guides l for Box Label

2,692 Views
steven_zhang
Contributor V

is there any guide doc for the below box label?

CAN接口,物料代码3 01 05 0003,规格TJA1051T 1,文晔,品牌NXP (2).jpg

 

0 Kudos
Reply
3 Replies

2,684 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @steven_zhang ,

From the picture you provide that the part should be TJA1051T. For the more information please kindly find it as the link.
https://www.nxp.com/products/interfaces/can-transceivers/can-with-flexible-data-rate/high-speed-can-...

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply

2,678 Views
steven_zhang
Contributor V

one of my custom want to know the labeling information about the nxp package box ,the TJA1051 is just the example ,there is another one as bellow:

单片机,物料代码3 01 05 0041,规格S912ZVMC25F1MKK,文晔,品牌NXP (2).jpg

 

0 Kudos
Reply

2,675 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @steven_zhang .

Thanks for your information.

You can get the below information from the picture:

PUID: product unique ID
QTY: quantity
TYPE : NXP part number
code NO. :12nc for the NXP INTERNAL USE
Or Scan QR code for more information as the picture.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply