When spi is used to communicate between NAFE13388b40bs and mcu, the mcu cannot read the information

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When spi is used to communicate between NAFE13388b40bs and mcu, the mcu cannot read the information

522 次查看
chen_xin
Contributor I

MCU and ADC chips communicate using SPI, with an ISO SPI isolation chip between them. There are six pins connecting the MCU and the ADC,including MISO, MOSI, NSS, CLK, DRDY,and INT. The DRDY pin is set to 1 when the ADC chip has completed data conversion. Currently, using a logic analyzer to capture these six pins, MOSI,NSS, and CLK are correct, and DRDY also sets to 1, but MISO is always at a low level. What could be the issue?

0 项奖励
回复
1 回复

436 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Not sure what kinds of read mode you select, but you can refer to datasheet Page41 7.5.4 ADC synchronization

0 项奖励
回复