VOH / VOL of PCA9617A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VOH / VOL of PCA9617A

530 Views
Jacky_L
Contributor I

Hi,

For PCA9617A, there is side A and side B. 

My side A is 1.8V, side B is 3.3V

But test conditions for Vcc=2.2V. 

I would like to know VOH / VOL of SCL /SDA.

Could you give me some advice?

 

 

 

0 Kudos
Reply
3 Replies

517 Views
Jacky_L
Contributor I

Hi

Yes, I saw VOL in datasheet, but  the test conditions is for Vcc=2.2V.  and my Vcc is 3.3V

So, I would like to ask about VOL of 3.3V.

 

thanks,

Jacky

 

0 Kudos
Reply

512 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jacky,

please refer to the notes on the top of the Table 5. The data are valid for VCC(A) = 0.8V to 5.5V and VCC(B) = 2.2V to 5.5V. For the 3.3V, you can expect, that the VOL value will be closer to the maximum VOL value, than for the 2.2V, but still within the boundaries. 

JozefKozon_0-1709814699129.png

With Best Regards,

Jozef

519 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Jacky,

for the VOL values for both A and B sides, please refer to the Table 5. in the PCA9617A datasheet

JozefKozon_0-1709812885897.png

The VOH value is VDD-0.4V. 

JozefKozon_1-1709812951407.png

With Best Regards,

Jozef

0 Kudos
Reply