Using PTN5150 in DFM only what then about VBUS_DET?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using PTN5150 in DFM only what then about VBUS_DET?

ソリューションへジャンプ
1,515件の閲覧回数
thomaskofoedhan
Contributor III

I want to use the PTN5150 for a DFM application only with 3A capability, but what should I do with the VBUS_DET pin?

Thomas

タグ(2)
1 解決策
1,380件の閲覧回数
thomaskofoedhan
Contributor III

Thank you Jose, for the answer. Clear and precise 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,380件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

When the PTN5110 controller is configured as a DFP mode application only, the VBUS_DET pin can be left unconnected.

Regards,

Jose

1,381件の閲覧回数
thomaskofoedhan
Contributor III

Thank you Jose, for the answer. Clear and precise 

0 件の賞賛
返信