The wet current of CD1020 exceeds the specification.Can it be used normally?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The wet current of CD1020 exceeds the specification.Can it be used normally?

531 Views
jingfang
Contributor IV

The maximum wet current configuerd for the CD1020 IO port is 16mA according to the specifications.

If the customer's switching current exceeds 16mA,the steady-state current is 20mA,and the impulse current is 50mA, does this situation cause IO corruption for CD1020?

0 Kudos
Reply
1 Reply

528 Views
guoweisun
NXP TechSupport
NXP TechSupport

That application out of specification ,don't suggest to do that!

0 Kudos
Reply