TJA1145A, TJA1145AFD, and TJA1145T/FD CANFD communication maximum baud rate issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1145A, TJA1145AFD, and TJA1145T/FD CANFD communication maximum baud rate issue

ソリューションへジャンプ
244件の閲覧回数
zhaoning
Contributor II

Hi NXP experts,

As shown in the pictures below, we have three types of CAN transceiver chips, TJA1145A, TJA1145AFD, and TJA1145T/FD. Currently, we have tested all three types of chips with silk screen printing, and they can all communicate normally at 5Mbit/s for CANFD communication. However, we found that the maximum CANFD speed for TJA1145 and TJA1145A in the manuals are 2M and 5M, respectively. We would like to confirm if all three types of chips we purchased can be used at a speed of 5M. Which datasheet corresponds to the model numbers of these chips, JTA1145 or TJA1145A?

 

zhaoning_6-1724382782394.png

 

zhaoning_1-1724382506214.pngzhaoning_2-1724382528168.png

zhaoning_3-1724382560264.pngzhaoning_4-1724382579252.png

zhaoning_5-1724382632365.png

0 件の賞賛
返信
1 解決策
228件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Zhao,

the TJA1145A and TJA1145A/FD can work reliably at speed up to 5Mbit/s. The older TJA1145 and TJA1145/FD can work reliably at speed up to 2Mbit/s. Please refer to the individual datasheets. 

https://www.nxp.com/docs/en/data-sheet/TJA1145A.pdf for TJA1145A

https://www.nxp.com/docs/en/data-sheet/TJA1145.pdf for TJA1145

The timings and reliability of the TJA1145 are not guaranteed above the 2Mbit/s.

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
229件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Zhao,

the TJA1145A and TJA1145A/FD can work reliably at speed up to 5Mbit/s. The older TJA1145 and TJA1145/FD can work reliably at speed up to 2Mbit/s. Please refer to the individual datasheets. 

https://www.nxp.com/docs/en/data-sheet/TJA1145A.pdf for TJA1145A

https://www.nxp.com/docs/en/data-sheet/TJA1145.pdf for TJA1145

The timings and reliability of the TJA1145 are not guaranteed above the 2Mbit/s.

With Best Regards,

Jozef

0 件の賞賛
返信