TJA1050 AEC-Q100 or higher qualification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1050 AEC-Q100 or higher qualification

ソリューションへジャンプ
778件の閲覧回数
Boris_Bloxsberg
Contributor III

Hi,

does the TJA1050T/CM,118 have an AEC-Q100 qualification and is it recommended for new designs?

regards

0 件の賞賛
返信
1 解決策
773件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, the TJA1050T/CM,118 is AEC-Q100 qualified and still recommended for new designs.

Originally the type was diffused in the ICN5 wafer fab in Nijmegen, that wafer fab closed end of 2010. Diffusion was transferred to Hamburg, that was the TJA1051T/VM. The present TJA1050T/CM (after the Hamburg fab stopped production of this process) is diffused in our 8 inch ICN8 factory, in Nijmegen, NL.

Best regards,

Tomas

元の投稿で解決策を見る

1 返信
774件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, the TJA1050T/CM,118 is AEC-Q100 qualified and still recommended for new designs.

Originally the type was diffused in the ICN5 wafer fab in Nijmegen, that wafer fab closed end of 2010. Diffusion was transferred to Hamburg, that was the TJA1051T/VM. The present TJA1050T/CM (after the Hamburg fab stopped production of this process) is diffused in our 8 inch ICN8 factory, in Nijmegen, NL.

Best regards,

Tomas