TJA1050 AEC-Q100 or higher qualification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TJA1050 AEC-Q100 or higher qualification

跳至解决方案
779 次查看
Boris_Bloxsberg
Contributor III

Hi,

does the TJA1050T/CM,118 have an AEC-Q100 qualification and is it recommended for new designs?

regards

0 项奖励
回复
1 解答
774 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, the TJA1050T/CM,118 is AEC-Q100 qualified and still recommended for new designs.

Originally the type was diffused in the ICN5 wafer fab in Nijmegen, that wafer fab closed end of 2010. Diffusion was transferred to Hamburg, that was the TJA1051T/VM. The present TJA1050T/CM (after the Hamburg fab stopped production of this process) is diffused in our 8 inch ICN8 factory, in Nijmegen, NL.

Best regards,

Tomas

在原帖中查看解决方案

1 回复
775 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, the TJA1050T/CM,118 is AEC-Q100 qualified and still recommended for new designs.

Originally the type was diffused in the ICN5 wafer fab in Nijmegen, that wafer fab closed end of 2010. Diffusion was transferred to Hamburg, that was the TJA1051T/VM. The present TJA1050T/CM (after the Hamburg fab stopped production of this process) is diffused in our 8 inch ICN8 factory, in Nijmegen, NL.

Best regards,

Tomas