Hi,
I have an OM17024(Evaluation Board of BGA3131) and I do not have the SPI to USB board and the SPI cable. I am looking to make a SPI cable. Can someone let me know the model/part number of the 10 pins header connector? It would be ideal to also know the model/part number of reverse gender of the header and the cable for the SPI cable.
Thanks
The connector is 2.00mm Pitch, Milli-Grid PCB Header, Dual Row, Vertical, Surface Mount, 10 Circuits, without Locking Window, with Center Polarization Slot. You can buy the full evaluation kit from our distributors