MRFE6VS25L & MRF1K50H Noise parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRFE6VS25L & MRF1K50H Noise parameters

697 Views
HarishRavichandran
Contributor I

We have bought MRFE6VS25L and MRF1K50H devices. I'm unable to find the noise related parameters like Rn(Noise resistance), NFmin (Min noise figure) and Yopt(Optimum Admittance) from the device data sheet. How can I obtain these values? I wanted these for my simulation purpose. Expecting kind help from the community. 

0 Kudos
Reply
1 Reply

642 Views
andrei_skok
NXP Employee
NXP Employee

We do not have noise data as we never tested the Noise figure on high power devices. Typical LDMOS NF's are in the 4dB to 5dB range, so one could expect these parts to have numbers close to those values.

0 Kudos
Reply