SPI cable for OM17024(Evaluation Board of BGA3131)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI cable for OM17024(Evaluation Board of BGA3131)

459件の閲覧回数
StevenC_Advintive
Contributor I

Hi,

I have an OM17024(Evaluation Board of BGA3131) and I do not have the SPI to USB board and the SPI cable. I am looking to make a SPI cable. Can someone let me know the model/part number of the 10 pins header connector? It would be ideal to also know the model/part number of reverse gender of the header and the cable for the SPI cable.

Thanks

0 件の賞賛
1 返信

410件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

The connector is 2.00mm Pitch, Milli-Grid PCB Header, Dual Row, Vertical, Surface Mount, 10 Circuits, without Locking Window, with Center Polarization Slot. You can buy the full evaluation kit from our distributors

https://www.nxp.com/products/radio-frequency/rf-amplifiers-low-medium-power/variable-gain-amplifiers...

0 件の賞賛