Dear Mr/Mrs,
I woud like to know the following characteristics of the SC18IS604PWJ component:
Temperature Junction maximum.
Thermal Rj-c
Thermal Rj-b
Thanks in advance,
Best regards,
Carlos Antón
Solved! Go to Solution.
Hi Carlos,
The thermal values for the SC18IS604PWJ component from our Package team. Here are the values:
Please note that these values are typical and can vary depending on the specific application and PCB design. For more information on the SC18IS604PWJ component, you can refer to the datasheet.
If you have any further questions or need assistance, please feel free to ask.
Best regards,
Hi Carlos,
The thermal values for the SC18IS604PWJ component from our Package team. Here are the values:
Please note that these values are typical and can vary depending on the specific application and PCB design. For more information on the SC18IS604PWJ component, you can refer to the datasheet.
If you have any further questions or need assistance, please feel free to ask.
Best regards,
Please help and fill below:
1: company name /location
2: project schedule
3: volume/annual
Hello guoweisun,
I would also need the Rj-a resistor value of the component. So as a sumarize:
Sorry for the inconvenience,
Best regards,
Carlos
Dear guoweisun
1: company name /location: Tecnobit, Madrid
2: project schedule: Design stage
3: volume/annual: up to 660 units
Hi Carlos,
Please accept our apologies for the delay in getting back to you, we currently do not have the required thermal values, but working on it and will update this thread as soon as I get them from our Package team.
Best regards,
Tomas