S32R45:Whether the DDR speed meets the requirements?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32R45:Whether the DDR speed meets the requirements?

1,158件の閲覧回数
Shi_test
Contributor III

Has anyone encountered this problem?

    On the basis of "RSDK_Multi_RFE_example_S32R45" I tried to run 1024-512-16 range with RF and SPT ( The output data format is "CP4Q_FMTA" ) . I found it OK to put the processed data on SRAM. But if i want to put the processed data on DDR it will not succeed. Because SPT does not return the completion callback "SptEcsIsrCb".  So I wonder if it is possible that the DDR speed is not as fast as the SRAM, causing the loss of chirp?

Shi_test_0-1689325795104.png

 

 

 

0 件の賞賛
返信
5 返答(返信)

993件の閲覧回数
WenChao
Contributor II

Hi I have the same quetion as you, dou you have some ideas to solve it?

0 件の賞賛
返信

760件の閲覧回数
Shi_test
Contributor III
官方说不建议将RF+range步骤的输出放到DDR。
0 件の賞賛
返信

1,132件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

If the issue is still relevant can you please submit a ticket at NXP.com so I can escalate this to RADAR team?

https://community.nxp.com/t5/HomeTest-Knowledge-Base/How-to-submit-a-new-question-for-NXP-Support/ta...

Best regards,

Peter

0 件の賞賛
返信

1,089件の閲覧回数
Shi_test
Contributor III

Shi_test_0-1690786995137.png

Hi Peter: 

I did what you wrote,but I don't have access.

What should I do in this case?

0 件の賞賛
返信

1,077件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

What exactly you did? There should be no restriction for ticket submit.

Just to have account created on NXP web.

Best regards,

Peter

タグ(1)
0 件の賞賛
返信