Hi,
I am using LS1046ardb board for one of my project, In that I want to build Yocto RFS with some more additional recipes. While adding Systemd recipe I am not able to build the Yocto RFS.
Please throw some light to resolve this problem. To add the systemd recipe into my root file system to make our life easier.
NOTE: I am adding Yocto recipes in local_arm64_devel.conf file and flex-builder -i mkrfs -r yocto:devel -a arm64 -m ls1046ardb is the command using to build the yocto root file system.
ERROR : NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'systemd' (but /home/auser/chethan/FR3_5/flexbuild_lsdk2004/packages/rfs/yocto-poky/meta/recipes-sato/images/core-image-sato.bb RDEPENDS on or otherwise requires it)
systemd was skipped: missing required distro feature 'systemd' (not in DISTRO_FEATURES)
NOTE: Runtime target 'systemd' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['systemd']
ERROR: Required build target 'core-image-sato' has no buildable providers.
Missing or unbuildable dependency chain was: ['core-image-sato', 'systemd']
Thanks & Regards,
Chethan GR
Solved! Go to Solution.
Hi,
After following the above steps, now I am able to configure the Systemd on my root file system. but after the adding the Systemd. in /etc directory all rc0.d rc1.d rc2.d rc3.d rc4.d rc5.d, rc6.d & rcS.d folder got removed so please provide me the solution its should have the both (means Systemd plus rcS.d). because i am going use both
Thanks & regards
Chethan GR
Please add "systemd-conf" to variable IMAGE_INSTALL_append in configs/yocto/local_arm64_devel.conf, then run the following command.
$ flex-builder -i mkrfs -r yocto:devel -a arm64
Hi,
After adding "systemd-conf" to variable IMAGE_INSTALL_append in configs/yocto/local_arm64_devel.conf, I got the yocto root file system. then same image I flash to the board.
I try to create the systemd service on /etc/systemd/system/ directory and service name is Startup@.service
Startup@.service is contains:
Description=Service Start
After=network.target
StartLimitIntervalSec=0
[Service]
Type=simple
Restart=on-failure
RestartSec=2
ExecStart=/bin/bash /etc/init.d/startup_service
RemainAfterExit=yes
[Install]
WantedBy=multi-user.target
After the creating Startup@.service file i try to enable the service using "systemctl enable Startup@.service" but this command is giving error.
ERROR : "-sh: systemctl: command not found"
Please let me know where missing while creating a systemd service OR is there any other way to create the systemd service means procedure.
Thanks & Regards,
Chethan GR
Please add the following line in packages/rfs/yocto-poky/meta/conf/layer.conf.
DISTRO_FEATURES_append = " systemd"
Then add "systemd" in configs/yocto/local_arm64_devel.conf and rebuild rootfs image.
Hi,
After adding DISTRO_FEATURES_append = " systemd" this in packages/rfs/yocto-poky/meta/conf/layer.conf. and "systemd-conf" in configs/yocto/local_arm64_devel.conf again give the build but No use. I am not able to get the systemd configure on my root file system
Please throw some light on same.
Thanks & Regards
Chethan GR
Please refer to the following procedure.
1. Please add the following line in packages/rfs/yocto-poky/meta/conf/layer.conf.
DISTRO_FEATURES_append = " systemd"
2. Please add "systemd" to variable IMAGE_INSTALL_append in configs/yocto/local_arm64_devel.conf.
3. $ flex-builder -i clean-rfs -r yocto:devel
4. $ flex-builder -i mkrfs -r yocto:devel -a arm64
Hi,
I follow the above steps but I did not get the Systemd configuration on my root file system.
Please help me to clear this problem and move forward.
Thanks & Regards
Chethan GR
Yocto uses sysvinit to do INIT by default.
Please add the following in configs/yocto/local_arm64_devel.conf to invoke systemd init function.
Hi,
After following the above steps, now I am able to configure the Systemd on my root file system. but after the adding the Systemd. in /etc directory all rc0.d rc1.d rc2.d rc3.d rc4.d rc5.d, rc6.d & rcS.d folder got removed so please provide me the solution its should have the both (means Systemd plus rcS.d). because i am going use both
Thanks & regards
Chethan GR