I am trying to make a USB3.0 Redriver using two PTN5150A and PTN36043A each.
I have added a block diagram on top of the attached schematic.
CC Controller does not operate normally in CONN2 of the block diagram.
I can only use Low=CC2 mode in External selection.
Is my schematic wrong?
Does NXP have a suitable redriver solution for Type-C?
My Redriver aims to support a Type-C connector capable of bi-directional flipping of both input and output using two PTN5150A and two PTN36043A.
Can I just set the DFP and UFP by controlling the PORT pin high and low?
If not, what setting should I do via I2C?
My Redriver connects like this:
PC --- Type-C --- Cable --- Type-C(flip1) --- PTN5150A --- PTN36043A --- PTN36043A --- PTN5150A --- Type-C(flip2) --- Cable --- Type-C --- Device