PT5150H - Supply drops

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PT5150H - Supply drops

386 Views
pafavre94
Contributor I

Dear NXP team,

I am using the PTN5150H for an UFP application without I2C.

I tested the following circuit :

PTN5150H_eval.PNG

SJ1 and SJ2 are shorted and C1=1uF.

R1=R2=R3=R4=10kohm

I connected a USB cable Type C to Type C (CBL-UC-UC-20BP - Cui) from my PC (a Microsoft Surface Pro) to the circuit using an USB Type C receptacle.

You can find attached the results:

CH1: VDD=VBUS, CH2: ADR

PTN5150H_VBUS_ADR.jpg

CH1: OUT2, CH2: OUT1 

PTN5150H_OUT2_OUT1.jpg

Can you explain this behavior ?

Do you have a clue why VBUS drops to less than 1V even though nothing consumes ? 

Note: This result is reproducible but does not always occur.

In fact, sometimes, VBUS is clean at 5V and ADR stays at 0V.

When unplugging and replugging the cable, the result described with the screen captures is reproduced.)

Thank you,

Best Regards,

Paul-Alexandre

 

Tags (1)
0 Kudos
Reply
1 Reply

378 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can try to add  below picture showed circuit to test again, for getting the  Logic to enable VBus discharge function :

guoweisun_0-1657692014878.png

 

0 Kudos
Reply