Hi, I'm new in NXP and I have a problem with uploading the example to the board.
I have a PNEV7462C dev board and want to upload phExCcid example using a J-Link or a divece as a mass storage. I've upload support packege and open the example with MCUXpress IDE, if I run the debug - the device works fine, but if I want to upload with RUN after uploading nothing works. Also I've tried with mass storage, upload EEPROM file separetly and bin file that was creating while building and nothing works.
I succesfuly open the needed project, but the problem is that the example works only in debug mode. When I use program flash or uploading using mass storage nothing works
Just checked the properties of this project, it programmed into flash. it should work without debug. But no print on debug console.
Regards
Daniel
Hi
Sorry I am not sure I catch your question, I would suggest you take a look at the um10883: PN7462 Quick Start Guider, it describes how to start and develop software and hardware with PN7462 family
https://www.nxp.com/docs/en/user-guide/UM10883.pdf
Regards
Daniel
I uploaded the code from this manual and succesfully run the needed example, but it works only in debug mode, if I program flash using JLink and MCUXpresso or using masstorage for uploading - nothing works
which demo you are using, let me try to reproduce this issue on my side
Regards
Daniel
This demo works without debugger, but you can not see the debug output in MCUXpresso console, since you stopped debugging. actually it works