PCF8566

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCF8566

694 次查看
ben_redmon
Contributor I

I am looking for a specification for the expected frequency min/max of the built-in internal oscillator (fosc) of the PCF8566 LCD Driver IC. The spec sheet only lists a range for fclk, which can be externally supplied or set to be fosc, as ranging from 125kHz to 315kHz. Does this mean that the internal oscillator (fosc) can have such a wide range of possible frequencies?

标记 (1)
0 项奖励
回复
1 回复

648 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Yes,the internal oscillator (fosc) can have such a wide range of possible frequencies!

0 项奖励
回复