PCF8523TK Circuit not acknowledge

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF8523TK Circuit not acknowledge

2,276 Views
rmkmani1001
Contributor I

Hi Team,

     I'm new to this forum.

     I have completed my design with PCF8523TK.

     When I try to communicate to chip using slave address (0xD0) with write bit.

     This chip is not acknowledge.

      Please   find my reference circuit and response for your reference.

Thanks and regards,

Mani

0 Kudos
Reply
10 Replies

1,963 Views
lisettelozano
NXP Employee
NXP Employee

Hello,

Correct, the pin 9 should be left disconnected/floating. Can you please try to disconnect it?

Another thing, the SDA and SCL lines should have connected a resistor on pull-up. Could you please double check that?

In your schematic, they don’t look to be on pull-up. Also, what size of resistors are you connecting to SDA and SCL?

We need to check if this can be a hardware issue with the device.

Have a great day,

Paulina

0 Kudos
Reply

1,963 Views
rmkmani1001
Contributor I

Hi Paulina,

               Thanks for your reply. Sorry for the delayed response, I was super busy in this week with office work.

    I will try to remove GND connection from Pin 9 and get back to you. (but its difficult, because of very tiny package).
   

     Note:
     a. SDA are SCL are pulled-up with 3K9  resistance, if not we can't able to get such wave forms (what i have attached in first mail). Am I correct..?

     b. I have connected 6, I2C devices with different slave addresses in this same bus, they are all works good [acknowledged and performed as expected].

thanks and regards,

Mani

0 Kudos
Reply

1,963 Views
lisettelozano
NXP Employee
NXP Employee

Hello,

Yes. However, the wave forms showed in your screenshot has some picks that can be noise. Please make sure that the resistors for the SDA and SCL lines are pull-up (connected to VDD as shown in the picture below) as per looking your schematic doesn’t look like they are pull-up.

 

pastedImage_1.png

pastedImage_2.png

Have a great day,

Paulina

0 Kudos
Reply

1,963 Views
rmkmani1001
Contributor I

Hi Paulina,
      Thanks for your info. I'm very sure, I'm using 3K9 pull-up to Vcc (_+3v3).
      All other I2C devices are working well as intended without any issue.
      I'm facing issue only with this chip. In above schematic R97 and R98 are 0 Ohms resistor for terminating purpose, I have added in my schematic.
      The SDA and SCL lines are tied with I2C Bus.

      FYI: I'm not yet tried with removing GND from pin 9, because it need a re-work. I have ordered couple Chips, I'm very sure the present chip will be damaged while removing from PCB. Once I have received new chips, then I will start to removing the existing chip from my Board and do the test.

     I will be keep you posted, if anything turned well.

Thanks and regards,

Mani

0 Kudos
Reply

1,963 Views
lisettelozano
NXP Employee
NXP Employee

Hello Mani, 

Sure, please keep me posted with any finding on your side. 

Have a great day, 

Paulina

0 Kudos
Reply

1,963 Views
rmkmani1001
Contributor I

Hi Paulina,
    Sorry for the delayed reply. I was super busy with office work.
    I hope I have identified the fault. The fault was while creating symbol I have swapped the SCL and SDA line..
    You can See in the above circuit diagram itself.

I have ordered small Piggy board [top- to-solder]. I will test it once PCB received.

thanks and regards,

Mani

0 Kudos
Reply

1,963 Views
rmkmani1001
Contributor I

Hi Paulina,

     Thanks for your reply and suggestion.
     I didn't wait for 2 sec, I will check and come back as soon as I can.

     but I'm very sure, I have followed as mentioned in datasheet 8.11.5 and within the  limits mentioned in table 49.

I have one more question.

I had a connection in pin 9 (exposed Pad) with GND, does it make any issue.? because we have note on page 5  in the datasheet as  "[3]The die paddle (exposed pad) is connected to VSS and should be electrically isolated."

Thanks and regards,

Mani

0 Kudos
Reply

1,963 Views
rmkmani1001
Contributor I

Hi Paulina,

     I have checked with more than 2 sec delayed after powered up. there is no change.. same as "Not acknowledge".

please share your clarification.

Thanks and Regards,

Mani

0 Kudos
Reply

1,963 Views
rmkmani1001
Contributor I

Hi Paulina,

   I forgot to inform you, I can have square wave pulses in pin INT/OUT. In this mean the oscillator work fine right..?.

Kindly share the solution , if possible.

I'm looking for solution last two weeks. I'm still scratching my head..

I have replaced two chips in my PCB, there is no difference. same as mentioned above.

Thanks and regards,

Mani

0 Kudos
Reply

1,963 Views
lisettelozano
NXP Employee
NXP Employee

Hello,

A couple of things:

  • We recommend to wait 2s after power-up to start working with the RTC so the oscillator can stabilize. Are you waiting such time?
  • Are you following the protocol mentioned in section 8.11.5 from the datasheet? Also, it is important to meet the I2C timings on table 49.

We have the following bare metal sample project for the PCF8523 which you can use as a reference on your design.

https://community.nxp.com/docs/DOC-340337

Have a great day,

Paulina

0 Kudos
Reply